2024-11-26 3:34 AM
I am wondering if ST could add a 3D model of the STLINK-V3 MINIE itself to the "CAD Resources". Currently, there are only STL files for ST's enclosure, but it would be helpful to have the 3D model of the PCBA itself to design other enclosures.
Solved! Go to Solution.
2025-04-11 12:32 AM
Hello,
It is now available on that page:
2024-11-26 5:14 AM
Hello,
thank you for your request,
I entered a ticket to see what can be done.
Internal reference: #197042
2025-03-01 3:55 AM
Hi, i need the same STEP model (STLINK-V3 MINIE),
we are developing a board whit a battery of 20 programmer mounted on the mainboard.
is it possible to have a link to download ?
Thanks in advance.
2025-03-03 1:18 AM
Note: Answered via PM.
2025-03-26 6:57 AM
Hello,
Was this request solved ?
Is it possible to get the STEP model ? (STLINK-V3 MINIE).
Thank you,
Noé.
2025-03-26 7:09 AM
Answered via PM.
2025-04-11 12:32 AM
2025-04-14 2:03 AM
Thank you Mike. It is very helpful that you’ve added this model. It is very much appreciated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.