2026-02-07 1:34 AM - last edited on 2026-03-02 4:50 AM by KDJEM.1
Hi,
I am facing an issue while connecting to my board using STM32CubeProgrammer and ST-LINK. I would appreciate any help.
Board: NUCLEO-F072RB
Programmer: ST-LINK (Onboard)
Software: STM32CubeProgrammer
Connection: SWD
ST-LINK Firmware: V2J46M31
Issue Description:
STM32CubeProgrammer is unable to detect the target MCU. It shows errors like:
Unable to get core ID
No STM32 target found
ST-LINK error (DEV_CONNECT_ERR)
Observed Details:
Target voltage showing around 0.29V
Connection mode tried: Normal (SWD)
Reset mode: Software reset
Speed: Reliable
Frequency: 4000 kHz
Log Messages (Important Parts):
Error: Unable to get core ID
Error: No STM32 target found!
ST-LINK error (DEV_CONNECT_ERR)
Error: Problem occurred while trying to connect
What I Already Checked:
USB cable and port
Reinstalled STM32CubeProgrammer
ST-LINK firmware upgrade option checked
Tried reconnecting multiple times
Questions:
Is the low target voltage (0.29V) the reason ST-LINK cannot detect the MCU?
Could this be a power supply or hardware issue on the board?
Should I try different reset modes (Hardware reset / Connect under reset)?
Any recommended debugging steps for this case?
Thanks in advance for your support.
2026-02-07 6:23 AM
> Target voltage showing around 0.29V
This is not enough voltage to run the chip. Changing the reset mode won't fix this.
Recheck your power settings. These are the defaults to power from USB:
If you haven't changed any settings and the board no longer works, it probably got damaged.
2026-02-10 10:29 AM
Hello @Visu
I recommend the following article describes tips to fix such errors encountered:
How to solve connection errors when connecting and programming the STM32 target board
Hope that helps!
2026-02-10 11:49 AM - edited 2026-02-10 11:52 AM
@Visu wrote:
Is the low target voltage (0.29V) the reason ST-LINK cannot detect the MCU?
Yes.
As @TDK said, the MCU cannot run at that voltage - therefore the ST-Link cannot communicate with it.
@Visu wrote:2. Could this be a power supply or hardware issue on the board?
Yes.
@Visu wrote:4. Any recommended debugging steps for this case?
Check the board's User Manual and schematics:
The fact that CubeProgrammer has the serial number & firmware version shows that it is communicating with the ST-Link.
Therefore power must be reaching the ST-Link.
So something is wrong between the ST-Link/USB and the MCU ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.