2020-04-30 11:19 PM
Takes about 15 seconds from click on the debug button in CubeIDE to the first break point ( the call to HAL_Init() ). Custom board, F401RTE, original ST Link V2, using SWD.
Would it be faster using a NUCLEO board ?
2020-05-01 1:21 AM
Subsequent code runs OK?
What's on the board? What is in the startup code? You surely can place a breakpoint at the reset vector's target and then single-step from there, can't you?
I don't use CubeIDE.
JW
2020-05-01 1:43 AM
Does you program sleep for extended periods? When not connecting under reset, debugger needs the CPU awaken to connect
2020-05-01 2:30 AM
Everything works fine.
The only issue is the time it take from pressing the debug button and until the program is reaching the first line in my program. A call to HAL_Init()
which is the first line in main(). The board is simple with only eeprom and RTC.
I didn't place any breakpoint it just stop there (on the line with a call to HAL_Init()) . It is OK to stop there automatically whe I debug. The issue is the time it takes to get there
Here is the printout from the debugger:
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 54FF72067880565340510267
ST-LINK FW : V2J36S7
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x433
Device name : STM32F401xD/E
Flash size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M4
Mass erase ...
Mass erase successfully achieved
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 54FF72067880565340510267
ST-LINK FW : V2J36S7
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x433
Device name : STM32F401xD/E
Flash size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a17956.srec
File : ST-LINK_GDB_server_a17956.srec
Size : 25376 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 1]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.213
Verifying ...
Download verified successfully
Erase and download are performed even when no change was made
2020-05-01 9:58 AM
15 seconds seems long. But Eclipse, on which CubeIDE is built, is very slow and clunky in general. Delays of seconds to do operations is not uncommon.
2020-05-01 10:26 AM
> Erase and download are performed even when no change was made
This. Mass erase is slow.
> I didn't place any breakpoint it just stop there (on the line with a call to HAL_Init()) . It is OK to stop there automatically whe I debug.
This is a temporary breakpoint enabled by checkbox "break at main" in the debug config.
If I understand correctly, CubeIDE debugger waits for the first breakpoint hit to fully start debugging.
Until the first breakpoint, it cannot do anything and all debug controls are disabled.
-- pa
2020-05-02 12:06 AM
Is there a better /faster way to debug both hardwae and software ?
2020-05-02 1:34 AM
As PavelA said above, avoid mass erase.
I don't know how, I don't use any of the eclipsoids.
JW
2020-05-02 7:19 AM
In my experience with several Eclipse-based IDEs, none of them have performed a full chip erase by default. Seems like yours is both doing a full chip erase, then doing an erase on individual sectors as well.
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 1]You'd need to disable the first full chip erase. Not sure how. Look for options in the run configuration settings.
2020-05-02 11:45 AM
Managed to remove the: monitor flash mass_erase from the debug configuration.
select Run from the main menu.
then select Debug configuration...
Click on the Startup tab
delete the:
monitor flash mass_erase
command in the initialization Command box
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.