STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer works fine with NUCLEO STM32F767ZI but fails to find NUCLEO STM32F446RE.

Hi, I have 2 Nucleo boards: NUCLEO STM32F767ZI (F4) and NUCLEO STM32F446RE (F7).I'm using macOS 10.15.4 omn MacBook Pro 2017 with STM32CubeProgrammer 2.4.0 and stlink tools from brew (GitHub.com/texane/stlib).When I plug in F4 over USB-C to USB-Mini ...

kj.obara by Associate III
  • 1921 Views
  • 6 replies
  • 0 kudos

Slow debugging start

Takes about 15 seconds from click on the debug button in CubeIDE to the first break point ( the call to  HAL_Init() ). Custom board, F401RTE, original ST Link V2, using SWD.Would it be faster using a NUCLEO board ?

ICohe.1 by Associate III
  • 4598 Views
  • 12 replies
  • 0 kudos

I made a PCB board with STM32F407VGT6 (MCU) + STM32F103CBT6 (Debugger). I get the message ''Usb device not recognizable''. Any idea why?

Hi all, I made a PCB board with STM32F407VGT6 (MCU) + STM32F103CBT6 (Debugger). I get the message ''Usb device not recognizable'' when I try to connect it to my computer via USB. I include the pics of my schematic. I followed the schematic of STM32F...

SSyme.1 by Associate II
  • 9353 Views
  • 11 replies
  • 0 kudos

STM32F030C8T6 internal protection of port PB8 and PB9 (FTf ports): Is voltage -0.35V with 100k series resistor a problem for the STM32?

We use the schematic attached to convert a 230 VAC signal to the STM32 level (low cost product). Maximum input high level is about 3.9 V. In worst case 5.4 V. This should not be a problem for the FTf pin because specification is VDDIO+4V = 7.3 V.But ...

MMuel.1 by Associate
  • 2507 Views
  • 4 replies
  • 0 kudos

Resolved! ST link error

Hello Team,I am using System Workbench for coding of STM32f30xx series micro-controller.I m getting some error on regarding St-link match frequency , that is below:-Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)Licensed under GNU ...

LACTIC by Associate II
  • 5774 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.