2022-01-07 4:51 AM
The STM32F407 is programmed with STMCube IDE and there is no error during initizalition of the functions; HAL_Init(), SystemClock_Init(); MX_USB_DEVICE_Init().
As I expect that virtual com port will be opened while the PCB is plugged into my PC, unfortunately it didnot happen.
What should I do?
2022-01-07 5:04 AM
Which OTG? If FS, DFU works? The same (presumably minimal) firmware works on a "known good" board such as Nucleo/Disco/Eval?
JW
2022-01-07 6:13 AM
Sorry for incomplete information. USB OTG HS. But actually I didnt use any Nucleo/Disco/Eval, I am using designed PCB
2022-01-07 6:37 AM
When the problem is localized, the transmit function of "CDC_Transmit_HS" returnes with "return USBD_BUSY".
uint8_t CDC_Transmit_HS(uint8_t* Buf, uint16_t Len)
{
uint8_t result = USBD_OK;
/* USER CODE BEGIN 12 */
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceHS.pClassData;
if (hcdc->TxState != 0){
return USBD_BUSY;
}
But, I want to say that the windows PC doesnot recognize the STM MCU ( no Virtual ComPort )
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.