2025-03-28 10:22 AM
I just received a NUCLEO-H503RB dev board, and while attempting to use the GPIO_IOToggle example program to test out the board, I could not run the debugger due to the error "ST-Link not detected." I went back to my NUCLEO-H7S3L8 board, it now receives the same error. A few days ago, I was able to program it.
I was able to detect the ST-Link with my NUCLEO-F446RE board.
Do I need to reinstall ST-Link or is there a way to force a firmware update on my two NUCLEO USBC dev kits?
Thank you.
Solved! Go to Solution.
2025-03-28 1:34 PM
Trying a 3rd cable was the key. It is quite touchy on the USBC cable.
With the 3rd cable, it shows up on my Device Manager and I can connect to it via STM32cubeIDE.
I am considering this issue resolved. Thank you for your help.
2025-03-28 11:01 AM
Are you using the correct USB connector?
Labeled USB STLK.
2025-03-28 11:39 AM
I have tried both USBC ports. One port, the LEDs do not light up. The other USBC port, near the header pins with the ST-LINK pins which are shorted together, blink through what appears to be a boot up sequence and then LED3 blinks at a regular pulse rate.
What should I try next?
Thank you.
2025-03-28 12:14 PM
Not sure, my NUCLEO-H503RB worked immediately.
"the header pins with the ST-LINK pins which are shorted together"?
Which pins are those? JP1 should not have a jumper.
2025-03-28 12:16 PM
JP5, SW_STLK pins are shorted to +5v.
2025-03-28 12:22 PM
5V_STLK shorted to +5V is the normal use case, board powered from ST-LINK USB connector.
2025-03-28 12:26 PM
What should I try next?
Is there a way to force a refresh of the NUCLEO's firmware? On the Silicon Labs kits, you can force an update of the firmware in situations similar to this.
2025-03-28 12:27 PM
Would using JP1 to reset the STLNK be worth a try? If yes, do I just short it out and then remove the short?
2025-03-28 12:33 PM
I believe STM32CubeProgrammer can be used to reprogram the ST-LINK, but I have not needed to do that.
2025-03-28 12:35 PM
"do I just short it out and then remove the short?"
That will reset the ST-LINK MCU, I don't expect it will solve your problem, though.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.