2019-08-08 2:59 AM
Hello
I'm pretty new to the STM32CubeIDE, and try to flash my test-program (a LED-blink programm) on my NUCLEO-F446RE developementboard. If i press the debug-button, the program is compiled, but then i get the folowing Error:
"Error in final launch sequence:
Error in initializing ST-LINK device.
Reason: (4) No device found on target.
Error in initializing ST-LINK device.
Reason: (4) No device found on target."
The frame of the code, i had generated with the HAL-codegenerator.
I have no settings changed in the IDE yet
Now I have no clue what to do, so hopefully somebody here can help me.
Thanks in advance
2019-08-09 4:18 AM
Hi
can you check that the power LED (LD3) is ON (RED LED). If not, can you check that the JP6 (IDD) is properly ON (remove it and put it back) and that JP5(PWR) is in the proper position (U5V).
See https://community.st.com/s/question/0D50X0000B6Q0SMSQ0/stlink-broken-after-upgrade-on-nucleo-card for similar issue.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.