2025-12-13 4:48 AM - edited 2025-12-13 5:11 AM
I am developing a TouchGFX user interface on a STM32U5G9 with a 24bit RGB LCD screen. I have developed the user interface on the STM32U5G9J-DK2 development board, where it works fine. I imported the TouchGFX project on my custom board the framework stops after the first full screen is displayed.
As a test I have added a start-up screen with two colored boxes and a image in internal flash. I have configured interactions to jump to the main screen after 3 seconds. When I set a breakpoint inside model.tick(), it triggers before 25 ~30 times before it stops triggering. The other threads of the application run as intended (ThreadX). If I look at the thread list in CubeIDE, the TouchGFX thread has state ready, and it's run count stops increasing after the first frame is displayed on the screen.
I compared both projects of the devboard and my projects in cubeMX, and I can't find any differences. I compared both IDE projects with winmerge, but also nothing found which could cause this.
My debugging so far gave me the following insights:
void OSWrappers::signalVSync()
{
UINT ret;
// Send the message only if the queue is empty.
// This call is from ISR, so no need to re-send
// the message if not yet consumed by threads
if (vsync_q.tx_queue_enqueued == 0)
{
// This is supposed to be called from Vsync Interrupt Handler
// So wait_option should be equal to TX_NO_WAIT
ret = tx_queue_send(&vsync_q, &dummy_msg, TX_NO_WAIT);
if (ret != TX_SUCCESS)
{
assert(0 && "Failed to Signal Vsync!");
}
}
}My touchGFX configuration:
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 1104K
FRAMEBUFFER_RAM (xrw) : ORIGIN = 0x20000000 + 1104K, LENGTH = 1904K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 4096K - 32K
EXT_FLASH (rx) : ORIGIN = 0x90000000, LENGTH = 32M
EEPROM (rx) : ORIGIN = 0x08000000 + 4096K - 32K, LENGTH = 32K
}
.........
FramebufferSection (NOLOAD) :
{
*(TouchGFX_Framebuffer TouchGFX_Framebuffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
*(Nemagfx_Stencil_Buffer Nemagfx_Stencil_Buffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
*(Nemagfx_Memory_Pool_Buffer Nemagfx_Memory_Pool_Buffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >FRAMEBUFFER_RAM
VideobufferSection (NOLOAD) :
{
*(Video_RGB_Buffer Video_RGB_Buffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >RAM#define RING_SIZE 1024 /* Ring Buffer Size in byte */
#define NEMAGFX_MEM_POOL_SIZE 24320 /* NemaGFX byte pool size in byte */
#define NEMAGFX_STENCIL_POOL_SIZE 389120 /* NemaGFX stencil buffer pool size in byte */
LOCATION_PRAGMA_NOLOAD("Nemagfx_Memory_Pool_Buffer")
static uint8_t nemagfx_pool_mem[NEMAGFX_MEM_POOL_SIZE] LOCATION_ATTRIBUTE_NOLOAD("Nemagfx_Memory_Pool_Buffer"); /* NemaGFX memory pool */
LOCATION_PRAGMA_NOLOAD("Nemagfx_Stencil_Buffer")
static uint8_t nemagfx_stencil_buffer_mem[NEMAGFX_STENCIL_POOL_SIZE] LOCATION_ATTRIBUTE_NOLOAD("Nemagfx_Stencil_Buffer"); /* NemaGFX stencil buffer memory */
I hope someone can point me in the right direction :)
Kind regards,
Robin
Solved! Go to Solution.
2025-12-16 3:10 AM
I fixed the issue. I was blinded by the touchgfx stopping. In the end it was threadx which was blocking due to another thread overloading the OS.
2025-12-16 3:10 AM
I fixed the issue. I was blinded by the touchgfx stopping. In the end it was threadx which was blocking due to another thread overloading the OS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.