2025-02-14 9:43 PM
I am traying to meassure a clcok frequency using STM32F103C8T6 board i am unable to capture. Please anyone solve my problem. This is the code i am using.
#include "main.h"
#include <stdio.h>
#include <string.h>
#define IDLE 0
#define DONE 1
#define F_CLK 72000000UL // System clock frequency for STM32F1xx
volatile uint8_t state = IDLE;
volatile uint8_t message[50] = {'\0'}; // Message buffer
volatile uint32_t T1 = 0; // First capture
volatile uint32_t T2 = 0; // Second capture
volatile uint32_t ticks = 0; // Time difference
volatile uint16_t TIM2_OVC = 0; // Timer overflow counter
volatile uint32_t frequency = 0; // Calculated frequency
TIM_HandleTypeDef htim2;
UART_HandleTypeDef huart1;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM2_Init(void);
static void MX_USART1_UART_Init(void);
int main(void)
{
HAL_Init(); // Initialize HAL
SystemClock_Config(); // Configure the system clock
MX_GPIO_Init(); // Initialize GPIO
MX_TIM2_Init(); // Initialize Timer 2
MX_USART1_UART_Init(); // Initialize UART1
// Start timer and input capture interrupts
HAL_TIM_Base_Start_IT(&htim2); // Start timer overflow interrupt
HAL_TIM_IC_Start_IT(&htim2, TIM_CHANNEL_1); // Start input capture on channel 1
while (1)
{
// Main loop does nothing, frequency is measured in interrupts
}
}
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef* htim)
{
if (htim->Instance == TIM2 && htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
{
if (state == IDLE)
{
T1 = TIM2->CCR1; // Capture first time
TIM2_OVC = 0; // Reset overflow counter
state = DONE;
}
else if (state == DONE)
{
T2 = TIM2->CCR1; // Capture second time
ticks = (T2 + (TIM2_OVC * 65536)) - T1; // Calculate elapsed ticks
if (ticks > 10) // Ignore very small intervals
{
frequency = (uint32_t)(F_CLK / ticks); // Calculate frequency
sprintf((char*)message, "Frequency = %lu Hz\n\r", frequency);
//HAL_UART_Transmit(&huart1, message, strlen((char*)message), 100); // Transmit frequency
HAL_UART_Transmit(&huart1, (uint8_t*)message, strlen((char*)message), 100);
}
state = IDLE; // Reset state
}
}
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef* htim)
{
if (htim->Instance == TIM2)
{
TIM2_OVC++; // Increment overflow counter
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
static void MX_TIM2_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_IC_InitTypeDef sConfigIC = {0};
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 65535;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_IC_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
sConfigIC.ICFilter = 0;
if (HAL_TIM_IC_ConfigChannel(&htim2, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOA_CLK_ENABLE(); // Enable GPIOA clock
// Configure PA0 as TIM2_CH1 input
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
2025-02-14 11:49 PM
Why not debug your code first? Check if is braek in
HAL_TIM_IC_CaptureCallback
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.