2018-10-22 5:49 AM
Hello,
we develop a product based on an STM32F765.
Is it allowed to add a debug interface like the ones on 32F746GDISCOVERY. This would make it easier for our customers to start writing their own firmware extension.
Thank you.
2018-10-22 6:19 AM
If your customers are not likely to have their own debug/programming tools, wouldn't it make more sense to provide a bootloader so that they can can program via UART or USB?
2018-10-22 6:32 AM
I would resort to a wiring of the debug pins as seen on the Nucleo boards (without the STLink part).
That would leave customers the option to connect other debuggers (like the J-Link).
You might ask ST if they sell you pre-programmed ST-Link MCUs. Pretty sure you will not get the firmware...
2018-10-22 6:52 AM
Agree: providing a standard debug connector is probably a better way to go.
http://infocenter.arm.com/help/topic/com.arm.doc.faqs/attached/13634/cortex_debug_connectors.pdf - the 10-pin, 0.05" is the favourite these days...
I don't think ST sell the chips.
If you really want to make your own debug adaptor, look at CMSIS-DAP - which is open source.
2018-10-22 8:41 AM
Thank you for your answers.
Of course the easiest way is to add a 10 pin or 20 pin CortexM pin header and tell the customers to buy a debugger interface of their choice.
Components for a STLink/V2 would be ~ 8..10€ and ST publishes a BOM and firmware update files - so my assumption was the design is free to use in a customer design, but I coudn't find this info.
2018-10-22 3:59 PM
>>I don't think ST sell the chips.
@STOne-32 Please consider selling licensed ST-LINK/V3 F7 parts
2018-10-22 7:01 PM
A big selling point for us developing off the Nucleo was the drag-and-drop via USB feature so we designed it in to our end-product. Sure it was similar to CMSIS DAP but in our mind it was a feature that was part of the ST/Nucleo ecosystem so off we ran.
Then when it came to finding the code we hit a brick wall. Eventually the wall came down and ST licensed out the code to us (binary, not source). That model has repeated itself across multiple companies over the last 4 yrs. Everything will depend on your relationship with ST on this but don't consider it an impossible issue.
Honestly it would have been easier if ST just sold the parts pre-programmed to us. ..not sure why they have not considered that instead of trying to stop the Chinese clones on the market.
2018-10-23 1:07 AM
Actually, the drag-and-drop is a feature from mbed.
https://os.mbed.com/handbook/CMSIS-DAP
DAPLink includes the drag-and-drop programming: https://os.mbed.com/docs/latest/tools/daplink.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.