STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use SWD without JLink/Debugger

Hi everybody,I need to connect to the SWD Interface of my STM32F0 without any debugger. I already studied the protocol itself and I am able to read the correct IDCODE of the MCU. Now I want to write to the CTRL/STAT Register. It seems that the target...

0690X000006CEDdQAO.png
ASieg by Associate
  • 937 Views
  • 0 replies
  • 0 kudos

Resolved! [SOLVED] ST-LINK Utility "Automatic mode" not working with debugger version V2.J29.S7 ?

The Automatic mode in the ST-LINK Utility hangs whenever I press the START button. I've seen on the forum similar problems with version J28. The solution was to downgrade the ST-LINK debugger to J27. Does the J29 version have the same bug?Is there an...

Problems with flashing into Nucleo32-l432kc

Hello,I have Nucleo32-l432kc board. When I am trying to run the ST-Link upgrade application it is showing ST-Link device not detected even though I connected the board. Later, when I am trying to flash the code it's not working, I assume because of t...

PPill by Associate II
  • 1237 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.