2019-11-17 10:55 PM
Here is what I did -
From CubeMX, I mistakenly change port configuration of port pin PA14 from SYS_JTCK-SWCLK to GPIO_Output.
Apparently this disabled the debug / programming channel of the target micro controller on the board.
Later I reset the port pin to its original function and tried to program the new firmware, but it doesn't work.
I get following error:
"Error in initializing ST-LINK device.
Reason: No device found on target."
Here's the complete console log -
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target no device found
Error in initializing ST-LINK device.
I know that the ST-Link is working normally because I was able to update its firmware.
When I keep the reset button pressed while the debugging session is being initiated, it shows the following message "Error in initializing ST-LINK device.
Reason: Target held under reset."
Is there any way to reset the JTAG / SWD channel on the Nucleo board?
Solved! Go to Solution.
2019-11-18 12:43 AM
Thankfully I was able to recover from this seemed to be serious issue.
Apparently I had remapped an SWD pin to generic I/O, after which the ST Link couldn't communicate with the device.
Resetting the I/O configuration, starting with a default project nothing at all would work.
I tried playing with lot of configuration setting in the Debugger where I changed the Debug Probe from 'ST-LINK (ST-LINK GDB server)' to 'ST-Link (OpenOCD)'.
This simply worked! I don't know how did this fixed it but later when I restored the Debug Probe to 'ST-LINK (ST-LINK GDB server)', it too worked!
If someone else faces this issue, this solution might help.
2019-11-18 12:43 AM
Thankfully I was able to recover from this seemed to be serious issue.
Apparently I had remapped an SWD pin to generic I/O, after which the ST Link couldn't communicate with the device.
Resetting the I/O configuration, starting with a default project nothing at all would work.
I tried playing with lot of configuration setting in the Debugger where I changed the Debug Probe from 'ST-LINK (ST-LINK GDB server)' to 'ST-Link (OpenOCD)'.
This simply worked! I don't know how did this fixed it but later when I restored the Debug Probe to 'ST-LINK (ST-LINK GDB server)', it too worked!
If someone else faces this issue, this solution might help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.