STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I built a brick

I designed a board based on an STM32F303CC and I am unable to upload any code to it. I'm using STM32CubeIDE with an ST-Link/V2 programmer. I've connected Pin 7 to DIO and Pin 9 to CLK. The board uses USB for it's 5V power supply which is transformed ...

MAkke by Associate III
  • 9459 Views
  • 12 replies
  • 0 kudos

ST-Link_CLI.exe get Device ID

I'm writing some code for our product flash programming via ST-Link_CLI.exe, because there are two kinds of STM32 MCU in one boards, one is STM32F417 another is STM32F09, two ST-Link connected to one PC via USB port. I would like to send command to g...

Resolved! How to factory reset Nucleo F103RB board? NUCLEO Board F103RB - Error in initializing ST-LINK device. Reason: No device found on target.

Here is what I did - From CubeMX, I mistakenly change port configuration of port pin PA14 from SYS_JTCK-SWCLK to GPIO_Output.Apparently this disabled the debug / programming channel of the target micro controller on the board.Later I reset the port p...

SShid by Associate III
  • 3525 Views
  • 1 replies
  • 0 kudos

Save SWO to file

Hi all,Is there any way to save SWO output to file using any official STM product?Best scenario would be to use st-link server.As we can have SWV it in STM32CubeIDE would be nice to have a option to save it to file.Regards,Pawel

PHryn by Associate III
  • 1600 Views
  • 1 replies
  • 2 kudos

Hello, I am using STM32H743ZI and try to load program into it from uVision using ST LINK, but get the following error. What could be the problem? Thank you.

Erase Done.Programming Done.Contents mismatch at: 08000360H (Flash=FFH Required=00H) !Contents mismatch at: 08000361H (Flash=FFH Required=20H) !Contents mismatch at: 08000362H (Flash=FFH Required=70H) !Contents mismatch at: 08000363H (Flash=FFH Requi...

MSun.5 by Associate II
  • 2267 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.