2020-12-30 2:34 AM
2020-12-30 6:18 AM
By "ST mini" do you mean STLINK-V3MINI? What does "ST link V3 debugger" refer to?
In any case, STLINK-V3MINI is very recent and should serve you well, unless you need to debug at less than 3V in which case you'll need STLINK-V3SET.
2020-12-30 8:08 AM
Yes i was asking abt stlink-v3 mini...and another one is STLINK�?V3 debugger/programmer....which one has better features?
2020-12-30 8:09 AM
STLINK-V3 SET*
2020-12-30 8:55 AM
"debugger hardware" or "debugger software"?
2020-12-30 9:04 AM
Both for the hardware and software
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.