Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi,i have problems to program my STM32F446. It was working some time before but today it didnt. by clicking download code to flash memory i get an error message, saying "error flash download failed" after that directly following "Error: Flash Downlo...
Hello,I made a circuit design for a college project and this is my first hardware design. Could I have a review of it before I send it out for getting PCBs.The microcontroller used is STM32F730R8T6. I am particularly interested in knowing if the USB ...
안녕하세요 .저는 STM32746G-DISCO 보드로 작�?� 프로�?트를 개발하고 있습니다.STM32746G-DISCO 보드�? st �?서 제공하는 �?�모 �?�미지 파�?� STM32746G-DISCO_Demo_V1.5.0.hex external loader(N25Q128A_STM32F746G-DISCO) 로 다운로드 하면 아래와 같�?� 0x90000000 번지 programming 할때 �?러가 발�?합니다.그래서 �?�미지가 나...
Hi! I have checked on Nucleo-F303K8's documentation that the required external power supply can be in a range of 3-3.6V. But what rechargeable LiPo battery can I use for this scope? I only found 3.7V ones!
Hello! I am trying to access the Virtual COM Port of my 32F746GDISCOVERY' board. Unfortunately, the the COM port is not listed correctly in my system (Ubuntu 16.04). This is the output of "lsusb -v"Bus 001 Device 012: ID 0483:3752 STMicroelectronics ...
Hi,I just got my H745i-DISCO board and started to tinker with ToughGFX right away. I got a test application loaded on the board, but once I disconnected the USB connection and reconnect it (USB connected to STLink USB Port on Nucleo board, power jump...
I have an STM32 Nucleo 32 (F303K8) and was able to use it before. But 1.4 doesn't seem to recognize the boards. I even connected STLink-v2 device and even that did not get identified.
STM32CubeProgrammer & ST-LINK/V2 & STM32F030I get "Error: No STM32 target found!" error regardless of what configuration I try. Log:ST-LINK SN : 55FF6F066675544945212587ST-LINK FW : V2J37S7Board : --Voltage : 3.99VError: No STM32 target found!The sol...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.