2022-03-08 11:26 AM
2022-03-09 10:12 AM
Seems SWD for you work then why you dont check 2MB flash ?
RevisionID isnt problem
2022-03-11 2:54 PM
Finally, Chip Programmed with Software STM32CubeProgrammer and St-Linl Programmer V2.
Installed firmware Pin2dmd.bin V4.33.
23:46:25 : Warning: Device changed, refreshing...
23:46:25 : ST-LINK SN : 0B330F1F731530303030XXXX
23:46:25 : ST-LINK FW : V2J39S7
23:46:25 : Board : --
23:46:25 : Voltage : 3.18V
23:46:25 : SWD freq : 4000 KHz
23:46:25 : Connect mode: Normal
23:46:25 : Reset mode : Hardware reset
23:46:25 : Device ID : 0x419
23:46:25 : Revision ID : Rev 5/B
23:46:25 : ST-LINK SN : 0B330F1F731530303030XXXX
23:46:25 : ST-LINK FW : V2J39S7
23:46:25 : Board : --
23:46:25 : Voltage : 3.08V
23:46:25 : SWD freq : 4000 KHz
23:46:25 : Connect mode: Normal
23:46:25 : Reset mode : Hardware reset
23:46:25 : Device ID : 0x419
23:46:25 : Revision ID : Rev 5/B
23:46:25 : Debug in Low Power mode is not supported for this device.
23:46:25 : UPLOADING OPTION BYTES DATA ...
23:46:25 : Bank : 0x00
23:46:25 : Address : 0x40023c14
23:46:25 : Size : 8 Bytes
23:46:25 : UPLOADING ...
23:46:25 : Size : 1024 Bytes
23:46:25 : Address : 0x8000000
23:46:25 : Read progress:
23:46:25 : Data read successfully
23:46:25 : Time elapsed during the read operation is: 00:00:00.006
Unfortunately, it doesn't work...
Thanks to all my friends for the time and support they have offered me.
2022-03-11 3:32 PM
>>Unfortunately, it doesn't work
That's a bit non-specific. The thread seems to lack much in the way of any context, or instructions you're trying to follow, or any details about the board. Looks to be one driving LED panel, but question talks about USB-DFU, then you use ST-LINK Clone, show memory with junk content and make declaratory statements about fake chips. Some People? It would be helpful to point at some actual web sites, or threads, or some contextual detail.
Aren't there more appropriate forums to be discussing this hardware.
Surely there should be some instructions, or diagnostic methods people are following.
Are you sure this is adequately powered? Not sure the ST-LINK clone provides a lot of current? Do the instruction indicate you should be powering things? Can you look at a schematic and confirm voltages at key points on the circuit or board?
2022-03-11 3:54 PM
ST-LINK Clone works and programs perfectly a old Pin2dmd Board with an old and Original STM32 Chip.
Greetings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.