2011-09-26 8:06 PM
Hi,
Just started playing around with my STM32 discovery board, and had a problem right away. I'm using atollic trueStudio IDE and trying to load a demo project(the one in firmware package), to my microcontroller. The thing is everytime I hit debug button It shows this in console:Starting server with the following options:
Persistant Mode : Disabled
LogFile Name : debug_log.txt
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Error in Initializing ST-Link device
I spent entire day searching web, if I could find a solution but no success yet. I found this page(http://www.atollic.com/index.php/kb/3-debugging/28-kb_st_link_connection_error
) on atollic website, have followed the steps but still no luck. So these are the things which I have already tried:- checked USB cable- tried running ST-LINK GDB server, same error- checked the driver installation, and updated to latest version- no disk letter issue, st link is using G: and it is vacantI have followed the user manual steps exactly still unsure what's wrong with my board. Any help appreciated. #debugging #st-link-gdbserver #driver2012-06-06 6:35 AM
Hello,
I have the same problem and i didn't find a solution, can somebody help me ? Florent2012-06-06 7:08 AM
You might have not yet installed the ST-Link USB driver.
The discovery boards have one integrated, either the old version V1 (VL_Discovery), or the new version (V2, all later boards). Usually, a ''new hardware detected'' window pops up under Windows. Just follow it (automatic installation, no access to internet required). This drivers can also be found here: (down at the page, under ''SW DRIVERS''2012-06-06 7:24 AM
Thank you your response, but i don't think the driver is the problem.
Unlike the original poster, I already ran programs on the board.While I was manipulating a DB9 connector for RS232 connection, I got a bluescreen on my computer. And since that day, the same error pop-ups everytime I try to launch a debug session : http://image.noelshack.com/fichiers/2012/23/1338825285-cc.png2012-06-06 7:46 AM
Bluescreens are sometimes refered to as BSOD...
Your Windows Registry might got corrupted or partially wiped out. I would completely remove the driver in the hardware manager, and reinstall it. I hope you have a backup. Perhaps you are lucky, but expect more maladies.2012-06-06 7:51 AM
Addendum:
If you had this RS232 on a USB/RS232 adapter, you might have damaged that USB chip in your PC physically. Often there are more than one USB host adapters in a PC. Can you try a USB port on another driver chip ?2012-06-06 8:05 AM
I tried other usb port nothing new. I even try to run the same program with an other PC and an other board, but i got the same error... If it is an error related to the code, I don't understand why, when I create a new project, I get the same problem.
2012-06-06 9:34 AM
If the code programmed on the STM32 is non conducive to SWD connectivity, try pulling BOOT0 High, and restart the board so it enters system loader mode.
2012-06-06 10:56 AM
''Error in Initializing ST-Link device
'' points to a problem with the stlink debug adapter, which is the bridge to your application, so to speak. If the host can't find the stlink, you don't have a chance to flash/debug your application.2012-06-07 7:05 AM
Thank you, I pulled BOOT0 high, it works with my coworker's board, but for me, a new error appears :
http://www.noelshack.com/2012-23-1339077525-cc2.png If nothing get better, I'll replace the board.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.