Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi All, I am facing a strange issue with the STM32H7S78-DK.I am using STM32CubeIDE for all of these tests (Version: 1.17.0, Build: 23558_20241125_2245 (UTC)) and of course STM32CubeMX (Version: 6.13.0-RC5 Build: 20241122-0809 (UTC)).Basically when us...
@Amel NASRI @Tesla DeLorean Hi! I have a question about the ADC WD. I am trying to use it, being triggered by a touchscreen, I have set it as follow: static void MX_ADC1_Init(void){/* USER CODE BEGIN ADC1_Init 0 *//* USER CODE END ADC1_Init 0 */ADC_A...
I'm trying program FLASH via serial bootloader using STM32WL55 USART1 The an2606 indicates thatUSART-RX is PA10 pin, connected to CN7-32USART-TX is PA9 pin, connected to CN10-19I connected the BOOT0 pin to 3.3VIf after reset I send 0x7f to LPUART vi...
Hello,I am trying to program STM32F411CEU6 based board using STM32Cube Programmer. If I try to flash the file through DFU mode it gives an errorErasing internal memory sectors [0 1]sector 0000 does not existsector 0001 does not exist Programming thro...
I Recently bought a STM32F411CEU6 . It was working fine till i shorted two pins by mistake.The STM IDE says no target found when i try to upload the code .Only the power LED turns on but the USER LED doesn't.(The ST-Link still detects my Blue pill pr...
i have this problem https://community.st.com/t5/stm32-mcus-boards-and-hardware/error-in-initializing-st-link-device-reason-18-could-not-verify/td-p/314096 that , attach chip photo it doesn't look like a counterfeit chip Open On-Chip Debugger 0....
Hello, We have been using this Processor for very long time in our 2 project stream.We are planning to use this part again, but for application suitability we need to verify this product as per our requirement.So, i wanted to ask is there any Evaluat...
I am wondering if ST could add a 3D model of the STLINK-V3 MINIE itself to the "CAD Resources". Currently, there are only STL files for ST's enclosure, but it would be helpful to have the 3D model of the PCBA itself to design other enclosures.
Hello,we have purchased multiple Nucleo H723ZG and H7A3ZI-Q. Since the beginning, connection problems with ST-Link are plaguing the project. It is impossible to reliably debug, because connection with the host can't be established via USB. We have ch...
I created this 3d printable base for the Nucleo-64 boards, to avoid damage to the bottom pin headers, reduce the risk of short circuits and as a convenient support during the prototyping and development process. I share it here hoping someone else wi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.