STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK-V3PWR to Nucleo board SWD

Hi,I am trying to link up a Nucleo-F411RE board to a STLINK-V3PWR unit via the SWD (CN6) header.I am going to make a breakout board for the connector. See image below, I am assuming that I do not have to connect T_VCP_RX and T_VCP_TX to anything on t...

Breakout_board_connection_diagram.png

Resolved! Did I break my Nucleo-C092RC ?

Hello everyone   i am currently working on a project with a NUCLEO-C092RC Board. With this Board i want to send OBD-II Frames to my car and receive reponses with data. I also use a LCD Display via SPI. But now i have a problem. i connected CANH/L wit...

Resolved! Getting started with 32F469IDISCOVERY

It looks like I have the 32F469IDISCOVERY board that looks to be powered ok via USB connector CN13, however the board doesn't appear to have demo software preloaded. COM LED LD6 flashes red. I note on the ST website that there is the 32F469IDISCOVERY...

alw by Senior
  • 1164 Views
  • 24 replies
  • 18 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.