Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello everyone,I’m using the STM32H747I-DISCO development board for evaluation and prototyping. I would like to know whether this board has undergone any form of EMI/EMC certification (e.g., CE, FCC, CISPR) or internal EMI testing by ST.Specifically,...
On the STM32H7B3I-DK, several STMod+ signals share two GPIO options (e.g., PA11/PA0, PC3/PD5 for SPI2/USART2). Even when I configure only one of the shared pins as a simple GPIO (e.g., output or input with pull-up), it doesn’t function — no toggling,...
we need to connect a camera to the STM32H745-Disco board. Our ultimate goal is to develop an application similar to the image_classification example from the STM32AI Model Zoo. Since we are unable to purchase another board, we would like to ask if it...
Hi,I'm trying to toggle a pin on my STM32H723 (LQFP144) using GPIO. According to the Nucleo-144 board datasheet, PE12, PE13, and PE14 appear to be connected to both CN10 (Zio) and CN12 (Morpho).However, when I toggle the pins to light up an LED, the ...
On the phase outputs why are there ground cutouts on the layout for this reference design. Is there a risk to cross couple to the ground plane with the switching noise or is it for thermal concerns?I've seen this in several ST ESC designs for drones ...
Dear all!this is the first time i design PCB for STM32H755, as my understand for direct SMPS that i design like attach file, really i don't know is it correct, so can you help take look and let me know if any mistake.
Been working on the Nucleo H5 dev board for about a month. Everything with the built-in ST-Link/V3 was fine until randomly yesterday, the board would no longer get out of reset when the ST-Link is powered. Board powers up and boots if getting powe...
Hello community, I have thiss board, the first one I'm designing from scratch on stm32 platform. I am able to connect and program just fine to some of the MCUs, but for the vast majority, the chip somehow gets fried before I can program it: I can'...
It's possible to set an interrupt priority for a pin in STM32F411 MCU, right? My PC13 pin (user button) is set to GPIO_EXTI13 and I want to give it the preemption priority 3 in the NVIC (STM32Cube IDE ver: 1.18.1) but it's seemingly not possible! Its...
Hello everyone,I am working right now in a project involving some of ST products. I have my custom HW board with a STM32G0B1 MCU for a specific functionality. In order to work with it and be able to program and debug my project, I was using two main ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.