STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Troubles getting started STM32H7B3I-DK

Hello, guys. I recently bought STM32H7B3I-DK and started playing with it. There are a few questions/issues I have:1) It seems that the board is recognized by the host PC only when it is directly connected to the PC's USB port. If I connect it through...

bojankoce by Associate II
  • 3950 Views
  • 9 replies
  • 0 kudos

Resolved! Error in initializing ST-LINK device. Reason: ST-LINK firmware upgrade required. Please upgrade the ST-LINK firmware using the upgrade tool.

It asks to re-connect STLINK and press "yes". Nothing happens after. I've tried to install STM32CubeProgrammer to upgrade manually, but I could not get it running.OS X 10.15.4 java 14.0.1 2020-04-14Java(TM) SE Runtime Environment (build 14.0.1+7)What...

IK_RSA by Associate II
  • 5128 Views
  • 4 replies
  • 0 kudos

wrong capacity

After upgrade ST-Link firmware to 2.37.26, the drive capacity did not display correctly. On the screen - to boards Nucleo-64 F446RE and G474RE

EMitu by Associate II
  • 773 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.