Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body *****************************************************************...
I tried to use ST Link V2 to program the STM32H750 but I don't got it working. And I read somewhere that debugging doesn't work with STM32H750. Is that true?
I am doing a pcb layout with a STM32L432KCU6 and using 100% of its 32 pins in my project. BOOT0 signal is on pin 31 on that MCU and in my schematic I have a digital output on that pin (PH3). There is no pull-down/up on BOOT0 on my design. Programming...
Hello,I'm doing the layout of a PCB with a STM32L433RCT6 . On the datasheet seems that this micro doesn't have a thermal pad. Also in the libraries I downloaded from Mouser , there is no thermal pad. I'm new with this family of microcontroller so my ...
To measure the current of the MCU on the Nucleo L073RZ there is an IDD header (JP6), on the Nucleo L552ZE-Q there is also a IDD header (JP5).I expect when I remove the header and leave is open (no current meter) that the MCU does not receive any powe...
Hi, I tried to upgrade the firmware for my ST-LINK 3 SET (using the STLinkUpgrade came with STM32CubeProgrammer) and something went wrong (didn't do anything special, just clicked "Open in update mode" and then "Upgrade"). Now its "Version" appears t...
I would like to plug RS485 on VCP STLINKV3. I try to plug RTS (VPC2) on DE, but I finally saw on that RTS/CTS cannot be controled by software... Can we plug DE by an other way ?I would you like to try GPIO control, do you have simple CLI or GUI ?Rega...
Hi,I'm currently using the NUCLEO-G071RB.I want to design a custom PCB including only the STM32G071RB MCU and a PMIC (without the STLINK part of the NUCLEO board).Is the STLINK/V2 compatible for replacing the STLINK part of the NUCLEO? Are there othe...
Hi , I use STM32H757IIT6 now ,but follow the STM32H757XI EVB's Power design. Use SMPS diretly supply model for Vcore. But when power up the system,the total current up to 500mA,and the CPU chip is very hot. I attach the sch ,...
I have been struggling for a couple of days with a STM32VLDicovery board. When I plug in the device it appears as 'USB Mass Storage Device.' I attempt to program it from visual studio 2019, using VisualGDB, and I get a messahe saying:USB Mass Storage...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.