2020-05-16 1:05 AM
Hey guys. I am facing with annoying problem. i have designed my own custom stm32 board with stm32f103cbt6 mcu. At the beginning, when i try to burn bootloader via stlink, I successfully did it and i could programmed my custom pcb via usb. the PC13 led was blinking with properly. but suddenly it goes. usb didn`t work and when i tried to burn bootloader again, stlink can not connect and it says the core is held in reset. do you have any idea about it? i have googled it several times, i found some solutions but they didn`t work for mine.
Solved! Go to Solution.
2020-05-26 12:04 AM
Update! the problem is absolutely about pcb. i checked all solder stuff and it works.
2020-05-16 1:55 AM
Double check all connections and solder joint. Cross check your debugging procedures against another board. Break down your test in little unit, testing a long chain broken somewhere is hard.
2020-05-16 4:32 AM
Try to connect under reset with ST-Link. If that doesn't work, check power rails. Sounds like a hardware issue.
2020-05-16 4:39 AM
I already tried to connect under reset mode, nothing change. I ll try your suggestions. Thanks for replies. If it works, i ll post the solution.
2020-05-26 12:04 AM
Update! the problem is absolutely about pcb. i checked all solder stuff and it works.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.