2020-05-19 1:40 PM
It asks to re-connect STLINK and press "yes". Nothing happens after.
I've tried to install STM32CubeProgrammer to upgrade manually, but I could not get it running.
OS X 10.15.4
java 14.0.1 2020-04-14
Java(TM) SE Runtime Environment (build 14.0.1+7)
What should I do?
Regards,
T
Solved! Go to Solution.
2020-05-20 12:47 PM
Download stsw-link007 and unzip. In cd in stsw-link007/AllPlatforms, run "java -jar STLinkUpgrade.jar"
2020-05-20 11:35 AM
Find a Windows machine. Download the standalone ST-LINK updated from ST website and update it.
-- pa
2020-05-20 12:47 PM
Download stsw-link007 and unzip. In cd in stsw-link007/AllPlatforms, run "java -jar STLinkUpgrade.jar"
2020-05-20 1:01 PM
Whole point of migrating to this Java nonsense from the previous native versions was to support/function multi-platform. Just shows poor execution and testing.
On Windows you often have to reset the target CPU, or disconnect it (jumpers), for the ST-LINK to go into DFU mode, and be updatable. Watch also for tool chains, or applications, taking ownership of the resource and blocking other apps from using.
2020-05-20 1:20 PM
When I tried to run ST Link utility on my old win machine - it did upgrade it to some version, but I still had to run upgrade, one more time, now on Mac with Uwe's answer:java -jar STLinkUpgrade.jar
It seems that in Apple vs Windows - it still shortens up to knowledge of terminal window command
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.