STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U083RCT6 drive level on 32.768kHz LSE

Good day. I am working on a 32-pin STM32U083KCU6. This requires the use of LSE 32.768kHz crystal. I referred to AN2867 as the oscillator design guideline.The LSE has the following specs:Shunt capacitance - 1.15pF,ESR - 70k,Load capacitance - 7pF.Calc...

racc by Associate
  • 1300 Views
  • 4 replies
  • 0 kudos

STLINK-V3PWR - BRIDGE Windows Linker

I'm working on some automation for our project using the STLINK-V3PWR. For that, I need to control the GPIOs. Based on the information from this page, I managed to get a working solution. Unfortunately, when compiling on Windows, I ran into a linker ...

Davren by Associate
  • 465 Views
  • 0 replies
  • 0 kudos

Resolved! T_VCC on STLinkV3 vs VCC on target

I have made an adapter that sits between the STLink V3 and the device that needs to be programmed, so that I can give T_VCC on the STLink side 3.3V from an external supply.So far I have used 3.3V as VCC on the target as well, but I am considering low...

TLin.5 by Associate III
  • 1220 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.