Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello everyone,I want to add external RAM to the NUCLEO-N657X0-Q. From the docs I see two options:FMC with PSRAM/SRAM or SDRAMXSPI with HyperRAM or serial PSRAMBoth options seem to require wiring from the board headers (I couldn’t find a ready plug-i...
Hello,I'm currently trying to set up a simple project for the STM32N6750-DK. I want to toggle the red User-LED. I already worked a bit with ST-boards, so I did already started a new project in the CubeIDE and selected the LED as a GPIO-Output in the ...
Hi ST team,I'm working with the Nucleo-N657X0-Q board (STM32N657X0H3Q MCU) and running the nx_iperf example from NetX Duo. I’d like to understand what the SRAM clock frequency is during this example's execution. In the release notes, it’s mentioned t...
Hi everyone,I’m working on an audio recording project using the STM32H747-DISCO board with its built-in PDM microphone. The recording works — I can clearly hear my voice — but there’s a constant background white noise in the recording. I’m trying to ...
I am trying to set up a basic USB project on a NUCLEO-H7S3L8. It works okay with the HSI, but I need the HSE. I can see that the board has a 24MHz crystal fitted and resistors on SB14 and SB15. It's unmodified from the factory.HAL_RCC_OscConfig() alw...
Hello,I am using the STM32F429I-Discovery board with an MT9M001 camera module, and I am developing with STM32CubeIDE.I would like to display the live camera image on the built-in LCD of the F429 board.I have already connected the camera and can read ...
Hi, I’m implementing a self-powered USB 2.0 Full-speed device with an STM32H753XI and a USB-C connector.Could you please confirm that the attached schematic: Uses STM-recommended resistor values for the VBUS-sense divider on PA9 to prevent MCU damag...
Hello all, currently if I want to turn my cpus to 480 MHz and 240 MHz, I have to switch to ldo, and voltage scale 0, rev v. Using the default SMPS will give only 400MHz, I tried 480MHz with the wrong scale, SMPS, and successfully debugged the M7 but ...
good morning. since this morning, on my nucleoH755ZIQ I am trying to make work my UART connection. I followed the stm video on YouTube and did as said: connected USART 2 (doesn't USART 1 work?) and then implemented the simple code in the while lo...
Doing a short search, I did not find a board that conveniently fits my criteria for some future projects.These criteria are the following : - small form factor (not bigger than a Rasperry Pico, preferably smaller (Seed XIAO); - MCU preferably ran...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.