Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello everyone,I am desining a new board with STM32H747XI and i am stuck with power schematic.As i see, this mcu has internal smps regulator and we can use it several way but not as vdd supplier.I am cunfused about it. Can anyone help me thougt this?...
I am working on a project and plan to use STM32g030c6t6 as micro-controller. I am using STLINK v3 set as debugger for uploading the program. I am unaware of how will be the connection of the debugger and controller as I want to communicate through UA...
Hello All,I am trying to get UART programming to work reliably on an STM32H743.When I try and upload firmware I get the following output:" -------------------------------------------------------------------\r\n STM32CubePro...
I have one ST-Link/V2 and one ST-Link/V2 ISOL and I experience following difference which I did not expect:ST-Link/V2 provides 3.3V to power the target's µC on PIN 1 of the flat ribbon cableST-Link/V2 ISOL does NOT provide 3.3V on that pin with the s...
I want to use BOOT0 pin to select System Memory boot.nBOOT0 = 0, nBOOT1 = 1, nBOOT_SEL = 0 bits in user config are well programmed. Boot works well if my uC is coming from a POR or power cycle. But if I connect a ST-LINK to the uC and simply open the...
We use NUCLEO-H743ZI (old) and NUCLEO-H743ZI2 boards. The difference: ST-Link V2 vs. ST-Link V3.The same FW fails on newer ZI2 board with the ST-LINK V3 for the USB VCP UART transfer.Issue:I send files from terminal, or I use copy and paste of large ...
The Command is " ST-LINK_CLI.exe -c id=0 swd lpm crst -P "JM.bin" -V after_programming -score "When I do Program SM32f765 Using Device St-Link V2 & STM32Cube programmer GUI , then every time it is programmed .while randomly i get the issue with STli...
I have multiple programmers and I want to write a Script using this instead of the Serial numbers
I am testing the downloading method of source file from STM32CubeIDE on PC to Nucleo-144 boards(MB1137) using STLINK V3SET tool kit. The SWD connector(CN6) on MB1137 and the SWD connector on STLINK V3SET adapter board are used for the connection bet...
I'v just started working with some STM32F303Discovery boards to explore ideas for a high school physical computing class. The boards are brand new stock from Mouser I'm trying to get ITM messages and so far I'm striking out. I'm using OpenOCD on macO...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.