2021-02-22 12:00 AM
I am testing the downloading method of source file from STM32CubeIDE on PC to Nucleo-144 boards(MB1137) using STLINK V3SET tool kit. The SWD connector(CN6) on MB1137 and the SWD connector on STLINK V3SET adapter board are used for the connection between Nucleo-144 boards(MB1137) and STLINK V3SET.
As the downloading test, the download has been successfully done in case of Nucleo-F429ZI and Nucleo-F767ZI. However, the download has been failed in case of Nucleo-F746ZG, and the error messages after download are shown in the attached file.
So, I want to know why the errors occur when the source file is downloaded from STM32CubeIDE on PC to Nucleo-F746ZG board using STLINK V3SET. I want to know why the errors occur only in case of Nucleo-F746ZG.
I want to know the downloading method of source file from STM32CubeIDE on PC to Nucleo-F746ZG board using STLINK V3SET tool kit.
The testing configurations and the test results are shown in the attached file
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.