Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, We are using a customized board with stm32l4x MCU. A QSPI flash is connected with MCU. Trying to program qspi flash using ST Link Utility with External Loader. Somehow we are able to manage to program the qspi flash. Problem statement is, if I do...
Hey, I try to connect to STM32G0316-Discovery board from STM32 ST-Link Utility but no connection can be etablished. Err-Message is: "Can not connect to target! Can't reset the core."Software is okay, driver is okay (other boards work), onboard stlink...
Hello, I bought a NUCLEO-L552ZE-Q and tried to connect with STLINK Utility . But STLINK Utility rejects.08:57:29 : ST-LINK SN : 066CFF505352716587121640 08:57:29 : V2J37M26 08:57:29 : Connected via SWD. 08:57:29 : SWD Frequency = 4,0 MHz. 08:57:29 ...
We're using the STM32 Nucleo-L4R5ZIThe issue is that whenever we try to check the ST-Link using STM32Cube Programmer or ST-Link Utility, it won't connect to the board.We kept getting errors like"STLink USB Communication Error""No STM32 Target Found"I...
Attached please is the connected equipment, installed software and the error message.
Should be a fairly easy one, but wanted to ask first: the built in T_VCP_RX and T_VCP_TX show the opposite logic input/output to what I'd expect (Rx shows as an output) in table 6 of the user manual UM2502. So would I connect my target Rx pin to the...
Hello,I want to connect CMWX1ZZABZ-072 with ST-Link, but it doesn't works. CMWX1ZZABZ-072 has a break out board which can program with arduino core.But I want advanced programming. So I want to program on Keil.I tried to connect CMWX1ZZABZ-072 with S...
HI, I have trouble with downloading code in MCU STM32F103 (Blue Pill) by ST-Link v2. I have also try to download, read, erase MCU by STM32CubeProgrammer and it works correctly.Project was made by STMCube as Atolic project and after that it was conver...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.