Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
We have a STLink v3 Mods which is not capable of programming any STM32H7 MCU. The programmer works fine with G4s, F3s, F4s and L4s. Using the STM32Cube Programmer and 4kHz as a connection speed works fine for reading and writing. Higher speeds do not...
Hi All, I am working on a project which involves stm32l433RCT6P, LCD (4 x 28), GPIO, RTC and low power consumption. I have finished developing whole applications and now working on exploring the low power modes of the mcu. As per my recent findings, ...
I absolutely cannot understand how the normal loading of the program on the B-G431B-ESC1 board occurs if, due to the use of timer 4 as an input for Hall sensors according to the boot0 (PB8) circuit, it is pulled up to 3.3V through a resistance of 10k...
Hello,I'm working on the STM32F769I-EVAL.In the User Manual 2035, version 3 (last version), on the SDRAM schematic, the address pin are mapped such as:A0 to A11 are connectedA12 and A13 are not connectedA14 and A15 are connectedSo I have some questio...
Hello, after I read some topics here and on Google, is not clear for me where can I find the FW hex content to flash to recover an STLINK-V2 or to create a new one programmer home made.At least bootloader FW hex, and after that to update this on STM3...
In the debug configuration if i click on ST-LINK S/N and click on Scan, i get the serial number so something seems to be working
So I wanted to program today and opened ST_Cube_IDE, connected my board to my PC and it was flashing red. It didn't respond to me sending information through a terminal, so I debugged my program and uploaded it (it should have already been in memory)...
When preparing to set the option byte, it is found that the read protection setting is at level 1 and cannot be changed to level 0. Then, it cannot be applied when preparing to apply, as shown in figures 5
Hi,I am trying to use Ethernet with STM32H745XI Discovery board and try to find out, if default board configuration can be used or I need to redirect Q-SPI to pints to Ethernet. Unfortunately the documentation description is not clear - should be thi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.