Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I would like to use the stlink/v3 on the Nucleo144 stm32h7a3 board to program/debug my board is this possible? what do I need to connect?
I have two nucleo stm32f303re boards. When connected to PC one shows up as mass storage NODE_F303RE(F:). The other one shows up as NOD_F303RE(F:). Missing 'E'. Changing the windows label works but is only temporary. How can I change it in the ST-link...
Hello,I‘m trying to power up my development board with a external 5V power source. Is it possible to use the on-board ST-Link via USB at the same time? Thank you for your help. Best regards.
I have a problem with the connection. Yesterday my board stopped working (there is a file FAIL.txt: "The interface firmware FAILED to reset/halt the target MC" at board disk). I've done some research on how to fix it, but neither pressing reset nor c...
I run into this problem every time I debug. No matter what I did I couldn't fix it. Even though I selected Debug configuration>Debugger>ST-LINK(OPENOCD) and Reset mode>software system reset it still works. I made a chip earese from the ST-LINK UTILI...
Hello, I am working on NUCLEO-L552ZE board which has STM32L55 Cortex M33 MCU.I can program the device using Keil IDE using ST-Link Debugger option. But I would like to program the device using ST-Link Utility or STMCubeProgrammer. ST-Link Utility can...
I have a stlink v3 mini and it gets very hot only when connecting to the usb port without connecting anything to the debbuger terminals, even so I connect it to the card to program and program without problems, but after a few minutes, it sends conne...
Hi,Master:platform: STM32G030C8T6Block diagram: As shown in the following diagram, STM32G030C8 as a battery cabinet communicates with 6 power banks through SDA_X. In addition, USART2 (Tx/Rx) communicates with the host, and USART1 (Tx_1/Rx_1) communi...
I am setting up a STM32G4 based USB self powered device with CubeMX. The CDC/ACM stack nearly runs fine. How shall I implement VBUS handling? The part has no dedicated VBUS pin. So some app notes suggest to connect VBUS to a GPIO-extInt or ADC and im...
Hello,I am using STM32G030F6, use HSE, but when I set the system clock, PA14 change to OSC_IN but while PA15 change to OSC_EN, and I can't find any specification of this definition, can I use it as OSC_OUT?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.