2021-09-30 4:01 AM
Hi,
I am trying to use Ethernet with STM32H745XI Discovery board and try to find out, if default board configuration can be used or I need to redirect Q-SPI to pints to Ethernet. Unfortunately the documentation description is not clear - should be this done or should be this done only for Half-duplex operation. Is it possible to use RMII configuration?, in documentation has been written - it is connected with MII, but Microchip PHY support also RMII.
I am not hardware guy and have never worked with Ethernet previously.
So the 2 main question:
Thank you in advance.
Documentation reference:
Best regards, Dima
Solved! Go to Solution.
2021-10-26 6:21 AM
Hello @DSvit.1
Q-SPI and ethernet share some pins even when using RMII. Therefore, it wouldn't be possible to use ethernet without following the application note instructions.
BeST Regards,
Walid
2021-10-26 6:21 AM
Hello @DSvit.1
Q-SPI and ethernet share some pins even when using RMII. Therefore, it wouldn't be possible to use ethernet without following the application note instructions.
BeST Regards,
Walid
2021-10-27 12:55 AM
Hi Walid,
Get it worked !!!, thank you very much
Best Regards, Dmytro
2021-10-27 1:49 AM
Hello @DSvit.1 ,
Nice to here that and glad to help you :smiling_face_with_smiling_eyes:
Please click on Select as Best if my post fully answered your question. This will help other customers with the same issue to find the solution faster!
BeST Regards,
Walid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.