Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi all,I've tried every example I can find to send data to a terminal using UART on my Nucleo 144. Every time the code builds fine but there is never anything on the terminal, and the code doesn't get stuck anywhere it runs fine.
A PC app sends a reset command via USB. In the main app I use HAL_NVIC_SystemReset() to reset the board. If I use HAL_NVIC_SystemReset, windows loses USB com port and does not re-enumerate port unless I plug out and plug in USB cable. The PC app talk...
I already read this post with no success: https://community.st.com/s/question/0D50X00009Xka0fSAB/problem-with-the-nrst-pin-in-a-stm32f100cbt6I tried to design a simple board with a STM32L021K4 and to program it with a STLINK-v3 MINI. I got the follow...
STM32H7B3I-DK - Discovery kit use NX3215SA-32.768KHZ-EXS00A-MU00525 Crystal. Crystal Load Capacitance is 6, 9, 12.5 pF but STM32H7B3I-DK - Discovery kit use 1.5pF. Why it use different load capacitance.
I am using below componnet toolsMCU: STM32H7B3IIT6IDE: STM32CubeIDE Version: 1.9.0CRYSTAL: RT3215-32.768-12.5-TR ( 32.7680KHZ 12.5PF)I work with internal RTC. I will use for clock. But RTC clock behinds real clock. While the product is running, the l...
HiI wished to use my Segger J-link Pro to debug my Disco' Board, but when I connect using CN12 the Segger Spring Pin header it won't connect to the target, although the IDE and Programmer can "see" the j-Link probe. I read the board's user manual (UM...
Hi,I'm interested in hardware connection of STM32U5 and Smart card. They can be connected directly or there need to be Smartcard Interface circuit between (like ST8024)?Thanks in advance,Nenad
I just received 2 STM32L053 Discovery evaluation boards. Is there a demo preloaded on the board? What is it supposed to do? After I plugged power into USB ST-LINK, the first board cleared the display while the second did not. Then the boards do nothi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.