STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDRAM doesnt work properly

Hi.Im using IS42S16400J SDram.It was working fine when i first mounted it(its my own pcb design).But there was some problem with the i2c pins so i had do unmount the stm32h745 and mount it again.Now with the same code the sdram is not working fine.Th...

I have bought new stm32l562E-DK board recently, I have written embedded rust code to blink an led. the compilation is proper binary file generated. When I Flash it is showing this error. Please help me out.

sarathk@sarath:~/Desktop/project/open_s_projects/rust_projects/stm32l/led_blink$ probe-run target/thumbv7em-none-eabihf/debug/led_blink --chip stm32l562qeixqError: Error while flashingCaused by:   0: Something during the interaction with the core wen...

bsara.1 by Associate II
  • 6338 Views
  • 13 replies
  • 0 kudos

Resolved! Can I program STM32 U585AII6Q with ST-LINK/V2?

I made my own PCB with STM32U585AII6Q and there are pins SWCLK, NRST, SWDIO, GND, VDD which I connected to the ST-LINK/V2. When I try to program STM32 U5, I always have error "No device found on target".Is there a problem with ST-LINK/V2, do I need t...

ASavi.3 by Associate II
  • 1706 Views
  • 3 replies
  • 0 kudos

STM32 PCB Design

Hi,I am trying to create the PCB design of Nucleo32, the small one, I have created the prototype, where I have interfaced few sensors with it and now I want to design the final PCB, to give it a product shape, so my point is can I get the PCB design ...

AJame.4 by Associate
  • 2224 Views
  • 3 replies
  • 0 kudos

Resolved! Uploading code to STM32G030F6 IC

Hi all.I am having some trouble with communicating with an STM32G030F6 IC. I am using STM32CubeIDE to code and STlink-v3 mini to upload the code. The SWCLK and SWDIO pins are being used to upload the code. 3.3V is being supplied from elsewhere and th...

0693W00000Nq4anQAB.png
SRauf by Associate II
  • 1760 Views
  • 2 replies
  • 0 kudos

ST-Link V2 DLL Error in STM32CubeIDE

Hi there, I'm trying to debug an application running on a custom board with an STM32L073RZ on board. I can connect to the board and programme it using both STM32 ST-Link Utility and STM32CubeProgrammer. I'm using a JTAG to SWD adapter board.However, ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.