STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why do I need ST-link for STM32CubeIDE when the Arduino editor doesn't seem to need it?

I've just started with STM32s and have to say I'm finding the whole toolset incredibly confusing. I've managed to put together a first USB host project in STM32CubeIDE after doing a very simple one in the Arduino IDE very easily, but now I seem need ...

Nello by Associate II
  • 10511 Views
  • 7 replies
  • 0 kudos

Resolved! [Solved] SWD pins used by mistake in code, now locked out of chip (G030F6 - TSSOP20). How to revert?

By mistake, I ended up setting PA14 (SWCLK) as an input GPIO. Didn't catch the mistake until after the MCU had already been flashed. So, after that I can't connect to it anymore using ST-Link.Since I'm using a STM32G030F6 (TSSOP-20) chip, for this ch...

RMaia by Associate III
  • 5160 Views
  • 6 replies
  • 0 kudos

EVSPIN32F0601S3 kit

Hello, I recently purchased the EVSPIN32F0601S3 board and tried debugging via onboard ST-link, debugger could not connect with the main IC. I then connected the AC supply to the board, on turning on the supply the board just blew up. Kindly help me t...

RAlph.1 by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

Resolved! Wrong pins for CAN_RX and CAN_TX

Hello, I have found out that connection from transceiver pins CAN_RX and CAN_TX are connected to CAN_TX and CAN_RX.I mean :from CAN transceiver to stm32f105CAN_RX -----------------------------> CAN_TXCAN_TX------------------------------...

NASI by Senior
  • 2729 Views
  • 4 replies
  • 0 kudos

Resolved! stm32h757i-eval can't connect stm32 target after selecting M4 for boot and deselecting M7

Hello,I have stm32h757i-eval board here. I've used stm32cubeprogrammer to edit OB where I've unselected M7 core from booting and left just M4 selected. This was done in intention to boot just M4 core and leave M7 core halted.When I modified OB this w...

kgardas by Associate III
  • 2229 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.