STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reset of the controller

Very new to ST and struggling to understand the basics. As posted in previous posts i am using the STSPIN3201 motor controller, i am trying to write the basic LED toggling program. From STSPIN32F0 data sheet i found the micro used is STM32F031C6. I c...

0693W00000NrRvqQAF.jpg 0693W00000NrRw5QAF.jpg 0693W00000NrRwFQAV.jpg
JDesi.1 by Associate II
  • 7848 Views
  • 11 replies
  • 0 kudos

STM32F407VET6 heats up

Hello!Yesterday I was using somesensor with the STM32, and today I realized that the STM32 and the voltage regulator heats up. Also my two alternative STlink connects and disconnects from the USB. I uploaded an empty project, but it still the same. U...

SGonz.2 by Associate II
  • 2060 Views
  • 2 replies
  • 0 kudos

Resolved! How to write plain intel hex to flash?

Hi,I would like to copy the exact contents of a hex file to the flash memory of my f446 nucleo, complete with byte count, address info ....Is there any way to do this? Using ST-Link I can only find options to actually flash the hex file or manually a...

gfxfloro by Senior
  • 12394 Views
  • 21 replies
  • 0 kudos

Digital inputs in STM32 boards ?

I am working on reading an External 3 bit parallel CMOS ADC (4-8 MSPS)(from MAX2771 board or Eva KIT) GNSS digital output. I want to read this digital output pins using the NUCLEO-H723ZG, I do not know if there is digital inputs pin in the board ?if ...

AElta.1 by Associate II
  • 2213 Views
  • 2 replies
  • 0 kudos

Failed to start GDB server Error in initializing ST-LINK device. Reason: (4) No device found on target.

Hello, I am using an STM32G031 Nucleo 32 board. Everything worked well. Following break point I lost the gdb server connection. Unable to reconnect, I made an update of the driver st link. I started under reset, reinstalled an old st link driver... I...

0693W00000NrCrUQAV.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.