2022-06-14 2:33 PM
Hello!
Yesterday I was using somesensor with the STM32, and today I realized that the STM32 and the voltage regulator heats up. Also my two alternative STlink connects and disconnects from the USB.
I uploaded an empty project, but it still the same. USB connection is also inestable. What can be the cause of this? Yesterday I didn't have this problems.
2022-06-14 3:02 PM
>>What can be the cause of this?
Something got electrically damaged.
Finger burning hot would suggest an internal short.
2022-06-14 4:25 PM
Well, the most recent change I made was connect a common ground and set up a pull-up resistor in UART Rx with:
GPIOA->PUPDR |= GPIO_PUPDR_PU << (2 * 10);Can this pull-up resistor make my STM32 finger hot?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.