STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSE clock is off by 5% on Nucleo-L4R5ZI

Hi, I made a minimum CubeIDE project for a Nucleo-L4R5ZI. It clocks the RTC from LSE using the X2 quartz (NX3215SA-32.768kHz-EXS00A-MU00525) and outputs a 512Hz calibration signal on PC13. The output frequency is only ~492Hz which is a deviation of ~...

SFahr by Associate III
  • 5277 Views
  • 11 replies
  • 0 kudos

Error: failed to erase memory

Hello thereI was trying to debug my stm32h750 with an stlink-v3 mini. I'm currently working with an external flash as my code area. The bootloader and external loader worked before, but suddenly I can't load code on my external flash. Does anyone kno...

SRebe.1 by Associate
  • 1627 Views
  • 1 replies
  • 0 kudos

ST-link driver

I have stm32F407 discovery board and I have downloaded and installed the ST_LINK USB driver on my laptop running window 10, but when I plug in the discovery board, the error message pops up saying the USB driver is not recognized, in the device manag...

0693W00000NrxeXQAR.png 0693W00000Nrxf1QAB.png
lzhan.21 by Associate II
  • 2176 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.