STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLink to MIPI10 cable?

A web search tells me I have a problem! My STM32 target has a MIPI10 connection for SWD debugging which works great with my I-jet probe. I now need to use an STLink but none of the supplied cables are for a MIPI10 target. Where can I buy such a cable...

Smoke came out of the MPU and when I connect it to the computer, the power light is on, but the usb device is not recognized.

I connected the 5v input of usb-ttl to the 5v output of the MPU, while the mpu was plugged into the computer and suddenly smoke came out. Now I get 2.8V from the 5v output of the MPU, 2.5v from the 3v output. Also in the debug circuit, r4,r10,r11,r14...

ASONA.1 by Associate II
  • 7672 Views
  • 18 replies
  • 0 kudos

Hello everyone, I'm having a problem with my 2 of STM32H745I-DISCO boards. Code could not come to main while(1).

I saw the problem when I use them for a basic LED Blink code. The Code got stuck in a while loop in SystemClock_Config() function. I tried lots of things.My __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1) will not return to SystemClock_...

Conformal Coating STM32L431CCY6TR

Hi TeamWe are currently working on ST MCU PN: STM32L431CCY6TR in our new project. Thus, I would like to check with ST whether this part is OK to be Conformal coated? The reason is, our PCB will need to be conformal coating after all the components ar...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.