STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L412 32.768kHz Crystal Layout Queries

Hello,We are facing RTC Drift as mentioned in previous question, So We have some queries regarding PCB Layout.1) GND of Crystal's Capacitor is connected to nearest GND Pin of STM32L412, should I connect this MCU GND Pin to Common GND Plane?2) How sho...

0693W00000YANQ3QAP.png 0693W00000YANQSQA5.png 0693W00000YANQwQAP.png
DBhut.1 by Senior
  • 2457 Views
  • 4 replies
  • 0 kudos

I am trying to understand and implement a method of reusable code, starting with STM32 projects. Any ideas on the best method(s)?

Hi,I am trying to implement a method of reusable code starting with STM32 projects. I have multiple micro controllers (F4, F7 etc) that will need to run the same application code. As STM generate the Drivers/HAL for me. Would I need to write API func...

JNoon.1 by Associate III
  • 3512 Views
  • 5 replies
  • 1 kudos

Resolved! SMPS: Necessary or Not?

Hello,I am working on a custom board design and we are looking into using the STM32H7B3IIT6 or the STM32H7B3IIT6Q. The main difference I've seen between the two is the Q-version removes some of the IOs to add an SMPS. I am trying to determine if that...

KMew by Senior III
  • 4280 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.