Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Data for the parts used are shown in the photo above.I made the calculation as above, but I am curious as to whether I obtained the CL value correctly. result)→ECS-.327-12.5-12R-C-TR (32.768kHz CLoad 12.5pF, Cs 5pF)CL1=CL2=(CLoad-Cs)*2=(12.5pF - 5p...
Hi, I just got the nucleo stm32G474RE board and I'm trying to run a simple code with the STM32CubeIDE through Linux ubuntu 22.04 the problem is that my laptop seems to not recognize the board when I am connecting it via USB port literally nothing hap...
First of all, I changed it to the corresponding part, but I would like to ask a question to confirm. Part selection was carried out as follows, according to the formula in the photo above.Even though I looked into the Gm value, I couldn't understan...
I am struggling to find a good way to identify the two COM ports the STLink-V3PWR provides. One is for direct communication with the power measurement unit and the other is connected to DEBUG for the target device(VCP).We need a easy way to identify ...
I have set up a UART on a STM32L152C Discovery board on bare metal. No Embedded OS but using HAL.I'm running a single thread. The UART is being configured as:huart1.Instance = USART1;huart1.Init.BaudRate = 115200;huart1.Init.WordLength = UART_WORDL...
Currently using Nucleo-H7A3ZI-Q to test the USB FS interface and using Cube FW 1.10.1 -Using Nucleo end as USB Device mode with CDC class. The schematics of the nucleo board tells me both the VDD50USB and VDD33USB is internally self powered and tied ...
HI all,I am currently trying to port the STM32 USB-PD Example to another Board with other firmware. And still running into issues, I am unable to solve :\1. I can not receive UART Data via HAL_UART_RECEIVE_IT, as the callback is not called.2. I can n...
Hello,I am brand new to STM32 parts.I have a STM32F407G-DISC1 eval board and am using STM32CubeIDE version 1.13.1. I am trying to get the FatFs_USBDisk application working with the board. I imported the project and tried to build it.I get the followi...
Hi there,I am running a board simmilar to the X-NUCLEO-SRC1M1 but with a different pinout at the MCU. More detailed, my ISense and VSense Pins are connected to ADC9 and ADC10 instead of ADC0 and ADC15.The example works with the nucleo Board just fine...
Just as an idea for others...According to figure 5 of the STLINK-V3SET user manual, I asembled the set including the adapter board. Alas, the enclosure then is no longer "enclosed". Nevertheless, I wanted to use the set in this way because of the bri...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.