2023-09-26 1:21 AM
Data for the parts used are shown in the photo above.
I made the calculation as above, but I am curious as to whether I obtained the CL value correctly.
result)
→ECS-.327-12.5-12R-C-TR (32.768kHz CLoad 12.5pF, Cs 5pF)
CL1=CL2=(CLoad-Cs)*2=(12.5pF - 5pF)*2
CL1, CL2 →15pF (14~16pF)
→ECS-120-8-36-CKM-TR (12Mhz CLoad 8pF, Cs 5pF)
CL1=CL2=(CLoad-Cs)*2=(8pF - 5pF)*2
CL1, CL2 →6pF(5~7pF)
2023-09-26 7:06 AM
Best to keep the discussion in a single thread. You can reply to your other post to add more details as needed:
2023-09-26 11:18 PM
we need to consider the track capacitors from crystal to MCU.
in this case the CL1 and CL2 value is less than your calculation.
anyway, the test accuracy is important when you get the board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.