STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H735 debug/flash problem

Hi, I have a board with STM32H735I.I can only detect the IC when boot0 is tied to 3V3 effectively putting the MCU into DFU bootloader mode. In this mode, I can flash it OK with stlink or even USB-DFU. However, once I tie boot0 to gnd the device won't...

Ksmol by Associate II
  • 2757 Views
  • 2 replies
  • 0 kudos

Lwip, netif_is_link_up

When running on the STM32 F746 eval board, the code does not go into the "netif_is_link_up(&gnetif)" function in the lwip.c file. For this reason I cannot ping. How can I solve this problem?

HS by Associate II
  • 3403 Views
  • 4 replies
  • 0 kudos

Read Protection Problem

Hello. I have an STM32F407 Discovery Board. I have been using the same board for years. Last time i used it i was experimenting a speed control of a DC Motor which i had done it many times. After i started debug mode my board strangely shut down and ...

CPU.PNG Device_Memory.PNG Read_Out_Protection.PNG

STLinkV3SET Back plate

I have an STLinkV3SET  which came with a secondary module and spacer.  When I connect them all together, I can't seem to get the back plate on.  I noticed the image on page 14 of the user guide shows how to assemble the modules, but does not show the...

LMorr.3 by Senior II
  • 1834 Views
  • 2 replies
  • 0 kudos

STLINK-V3 not recognized

Hello there,I have just obtained the STLINK-V3 device:I have installed the STM32Cube Programmer (v 1.3.0) *** the drivers that comes along with it. The problem is that I cannot find the device:There is no drivers missing, the device manager is "clean...

0690X000006CoGyQAK.jpg 0690X000006CoH8QAK.png 0690X000006CoIkQAK.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.