2026-01-17 4:24 AM
I have ST win BX1 development board and I am using Zephyr RTOS for my development. I am not sure, How can I use the WiFi module on this board.
First, the module is connected over SPI and I have tried to send some AT commands but I did not get any response.
So, do I need to update firmware first? my answer is no because it comes already with the firmware installed.
I tried SPI with CS pin low and WiFi-EN pin High.
2026-01-20 3:42 AM
Hello @urath
Have you already checked this repo on GitHub? STWINBX1_WIFI package enables the support for the MXCHIP Wi-Fi module mounted on the STEVAL-STWINBX1. See also the README, where the Wi-Fi firmware update procedure is explicitly suggested.
Best regards,
Simone
2026-01-21 5:32 AM
Hi,
I have done that process already.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.