2023-06-20 5:11 AM - edited 2023-06-20 10:15 AM
Hi! When I connect stlink v3 minie , lounch cubeide -> stlink upgrade , it only shows "V3", nothing more. I can't open it for upgrade.
Other embedded in nucleo boards stlink v3 works and can be upgraded (nucleo G431 and H723).
There is an error about permissions. But I don't think that's the case.
Its brand new device, never used, never connected to target, original.
There is possibility that cubeide didn't updated - so I will try to download latest and update. But chances are small for this.
What to try first?
Thanks.
Edit: it was indeed a failed update issue. Solved!
2023-06-20 12:33 PM
Do the update on a good Windows 10 or 11 PC, with good cables. Using the latest Cubeide version is a good idea.
2024-01-03 8:17 AM - edited 2024-01-03 8:18 AM
NO WAY ! I will stick with linux. It updates with no problems now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.