STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK-V3MINIE current draw

I am using a STLINK-V3MINIE  as a programmer with my custom board.The custom board has a battery holder, with 2xAA 1.5V each.A jumper is in series with the positive terminal of the battery holder, where I am using an ammeter.I measure a baseline of 3...

dhs by Senior
  • 1249 Views
  • 0 replies
  • 0 kudos

Finding JTAG/SWD location on custom PCB

Hey ST Community,A little bit of background knowledge. Aside from a few Arduino/microcontroller courses in college I am relatively new to coding and MCUs, specifically the ARM format. I currently work in the heavy machinery segment and am trouble sho...

20240502_094956.jpg 20240502_091123.jpg

Resolved! Using Timer Global Interrupt crashes board

I have an Arduino Giga (STM32H7). I'm trying to generate an interrupt on the Catch/Compare even of TIM5_CH3. TIM5 is set to one pulse mode and triggered as a slave to TIM1, they generate some PWMs; everything is working absolutely fine there. Also, I...

Pepijn by Associate II
  • 8133 Views
  • 11 replies
  • 1 kudos

Resolved! Does STlink support AD V2multi-drop SWD?

All STM32 CortexM7 and M33 have a ADI V2 debug unit. ADI V2 requires Multi-drop support, so that several SWD devices can be connected to SWD in parallel. Only with an activation sequence including the target-ID of that device to use selects the devi...

ILI9806 init DPI mode

Trying to make KD043WVFPA084-01-C015B LCD to work - custom board 32H735 chip. Display is from Startek that probably went under. Web page disappeared and no one answers emails. Display uses ILI9896E chip and as per data sheet it is setup for DPI mode ...

AS1956 by Associate II
  • 1495 Views
  • 1 replies
  • 0 kudos

Resolved! stm32h725vgt6 not able to Program

My updates schematic in this pin number 11 is now connected to gnd not to VDD This My schematic for your reference This is the error in cube MX. previously I had similar issue that time it was because of power supply.I don't know what the mistake in ...

Sakthi_Murugesan_0-1714451112678.png Sakthi_Murugesan_0-1713868456670.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.