Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello everyone,i'm working on a programm on a Nucleo-L031K6 that send data to a stepper motor's driver (Enable, Direction and Pulse).It's a basic program that receive instruction from a python script (i send frames). I've a callback function which is...
Hello Team,I want to achieve 7.5msps using three 2.5msps external ADC with interleaving method. So how can I achieve this with STM32h745 controller. below attaches some documentation. please anyone can provide some example code or guidance to achieve...
Don't know weather my Stm32F405 (new) needs a bootload or not? I have designed a custom stm32 board in order to detect my stm32 by the computer for the code uploading i connected my stm32 externally with a TQFP breakout board with my ST-LINK V2 , all...
Hi, For some time now I was using cheap bluepill and stm32f030-demo boards to debun my project with st-link probes. It all works perfect. But recently the stmf030 become too small, so I decided to replace it with stm32f070 (same tssop20 package as or...
Hi, I need to modify this schematic, I want to use one USB connection connected to an STM32. - When the STM32 is on Bootloader mode, A virtual com port will be open and I should have an option to save a mp3 file inside the external flash (GD25P32)- W...
I need to download the STM32F4DISCOVERY board firmware package for the MATLAB toolbox, but it's not available for download on the official website.
HelloI want to use the AHPI7292S board with the STM32F7508-DK board.Is AHPI7292S compatible with STM32F7508-DK board? Is there any study on this subject?
I am trying to test STM32F469I Disco, it has already external loader in Keil ready to useEverything works fine it connects to the external QSPI when uploading I do not have any break points defined so why I get this error message and I cannot debug.
Hi,I'm using the H753ZI board with 26 ADC inputs on ADC1 & ADC3.The ADC pins run in DMA circular mode and all inputs seem to work fine except one pin: PA2PA2 is configured like the other pins: Analog mode, no pull-up and no pull-downBut the pin seems...
Hi everyone,I'm a beginner in electronics design but I'd like to create my own PCB.I've designed a schematic around the STM32F0 microcontroller and would greatly appreciate any feedback you might have.The setup involves a board with one transmitter a...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.