STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

eStore Credit Card Charging

I ordered a stm32h755zi nucleo board from stm estore but my concern is after ordering $1 was charged and my card was a debit visa card. since my order is confirmed then when will the rest of the money I have to pay i need a bit help about that if the...

Asraful by Associate III
  • 2877 Views
  • 4 replies
  • 3 kudos

I2C

Hello I am new with STM32 boards. I have 2 STM32 boards, and I am trying to get I2C communication between them. The boards I use are: NUCLEO-G071RB as the master, and STM32F412G-DISCO as the slave.I success to send a response from the slave to the ma...

MichaelR by Associate III
  • 3230 Views
  • 8 replies
  • 0 kudos

ST-LINK not detected on windows

I have couple of nucleo-g0b1re boards with me. Lately some of the boards are not identified on my Windows 11 PC. Also the boards which failed to be identified on updated cubeIDE and STM32Utility are also not detected by windows' device manager. They ...

2024-04-25 14_47_00-Device Manager.png 2024-04-25 14_48_03-Device Manager.png
VRA1 by Associate
  • 3643 Views
  • 2 replies
  • 1 kudos

Help for I2C

Hello,can someone help me with a sample code for STM32F12G-Disco?I am controlling the SSD1306 via I2C, so an oled display 0x78.I just want to output a text on the dsiplay. This is a code excerpt. Most of it was done by code generation:#define ssd1306...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.