2026-02-24 3:52 PM - edited 2026-02-24 3:53 PM
Hello, I read somewhere that I can use the ST-LINK built into my H563ZI to program my custom cards with STM32F401.
Could someone help me figure out how to do this?
Thanks in advance.
Solved! Go to Solution.
2026-02-24 4:35 PM - edited 2026-02-24 4:36 PM
Older style Nucleo-144 boards had a breakaway programmer that could be used to program other chips. Newer Nucleo-144 boards like the NUCLEO-H563ZI do not have this feature and programming external chips is not supported. Sorry.
Programmers are cheap. Consider getting a STLINK-V3MINIE and putting a standard programming header on the board to debug and program.
STLINK-V3MINIE | Tool - STMicroelectronics
2026-02-24 4:35 PM - edited 2026-02-24 4:36 PM
Older style Nucleo-144 boards had a breakaway programmer that could be used to program other chips. Newer Nucleo-144 boards like the NUCLEO-H563ZI do not have this feature and programming external chips is not supported. Sorry.
Programmers are cheap. Consider getting a STLINK-V3MINIE and putting a standard programming header on the board to debug and program.
STLINK-V3MINIE | Tool - STMicroelectronics
2026-02-24 5:04 PM
Hi,
> I read somewhere that I can use the ST-LINK built into my H563ZI to program my custom cards with...
This is only true for NUCLEO-64 and NUCLEO-144 boards with embedded ST-Link v2-1 (on a breakable part of the board).
Even without breaking the board the onboard ST-Link can be used for other STM32 MCUs.
See https://www.st.com/en/evaluation-tools/stm32-nucleo-boards/products.html and check for "Tool Type" is "Nucleo-64" or "Nucleo-144" *and* "ST-LINK" is "ST-LINK V2-1".
All others (Nucleo-32, or "ST-LINK" is "ST-LINK V3E") can not be used this way (ST-Link not detachable).
Your NUCLEO-H563ZI is this kind ("ST-LINK V3E") , so no way to program another MCU with this.
You should buy an external ST-Link (please take care of a genuine one, not the Ali-whatever "ST-Link v2 mini...") or another NUCLEO with detachable ST-Link V2.
Embedded ST-Link V2 on NUCLEO boards support only target voltage of 3V or 3.3V and no virtual COM port for external targets.
I would prefer an external one. But keep in mind that an external ST-Link V2 does not support virtual COM port, while an external ST-Link V3 does, and V3 is faster than V2.
And keep in mind that there also faked external ST-Link V2 around; choose a trusted dealer.
2026-02-25 4:28 PM
Thank you for your guidance. To program my Black Pill with STM32F401CCU6, I used the BOOT method via UART, which worked successfully.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.