Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello,I recently purchased STM32 F4VE trying to print text on SWV but noting shows at port 0, shared all the necessary information below.Here's what i did :I am using generic st-linkv2 (version : 3.14.5) and STM32F407VET6 is in Normal mode (not DFU)...
I am using STM32CubeMX and keil 5 to program my Nucleo-32 board. When I try to download firmware packages in STM32CubeMX, it shows the connection lost issue. Here is the snapshot attached. I have tried to log in but again it shows connection lost err...
Hello I got two boards dead within one day. I used the first board for a while and it worked until I started to communicate via USART/RS232. After I faced with such a problem, I replaced the board with a second one and immediately got same result.Des...
Hello, Recently I have purchased an evaluation board "NUCLEO-G071RB" to program/debug our custom board using ST-LINK. After 4 time successfully attemps to program our custom board, the evaluation board came with follow error and it was impossible to ...
Dear STM32 Community, I hope this email finds you well. I am reaching out to seek assistance regarding some persistent flash errors I've been encountering with the STM32L496VE microcontroller. In my application, I'm utilizing the bootloader to write ...
Hi @Peter BENSCH I have a query regarding voltage compatibility of Quad single-pole single-throw analog switch from Nexperia 74HCT4066.The switch part is voltage compatible with STM32G431MB/ME series when analyzing VOH VIH VIL VOL relationships wit...
Dear All,Just now I have plugged my ST-Link v3 Minie in. Updated it via CubeIDE. All looks good.I might have overseen something (scanned the user manual), but the BTB (CN2) connector on my ST-Link v3 Minie gives 0V voltage between T_GND(6) and T_VCC...
What is the difference between ST-LINK/V2-1 and V2? Where can I buy v2-1?Or are you buying v2 and updating the firmware?
Hi All,Is there an errata for the STM32L5 Nucleo board?I need to use the SPI on port G which requires PG11 for SPI MOSI.However in the schematic for the board, PG11 is missing from the schematic symbol (see page 3) and there is a gap. The pin number...
Hi,I want to write data in flash using DMA. I TRIED USING HAL_DMA_Start() FUNCTION. DATA NOT WRITE IN FLASH. HOW TO WRITE DATA IN FLASH USING DMA IN SMT32G0B1RCT6.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.